App freezes on dealloc

This topic contains 4 replies, has 5 voices, and was last updated by Profile photo of Manzar Manzar 1 month ago.

Viewing 5 posts - 1 through 5 (of 5 total)

  • Author

    Posts

  • #10517

    Profile photo of Dani
    Dani

    Participant

    Using the ViewController of the demo application, if I put it inside my app, when I go back the app freezes without being able to do anything.

    I have tried other dummy projects and the error is always the same. It occurs when you open a ViewController that connects with FLIROne camera, when you pull back (with the back button of the navigation bar or by calling popViewController) the application freezes (doesn’t receives touches) and can only be finished manually.

    It seems that some process in the SDK remains open running in the MainThread which blocks it completely.
    It occurs with different camera models (Normal, PRO and PRO LT).

    Dani

    #10620

    Profile photo of Gavin
    Gavin

    Keymaster

    Hey Dani,

    I’m currently looking into this issue and should have a response this afternoon.

    Gavin
    FLIR One Community Support

    #10623

    Profile photo of Cal Loo
    Cal Loo

    Moderator

    Hi Dani and Gavin,

    Just wanted to acknowledge that this issue was escalated through our support system to tier 3 in Sweden for urgent response. We’ll resolve it offline via email but post the outcome here so others can benefit. Thanks for reporting it here!

    Best,

    Cal

    #11823

    Profile photo of Raffaele
    Raffaele

    Participant

    Hi, it keeps freezing. It’s been 5 months since your last response.

    #12162

    Profile photo of Manzar
    Manzar

    Participant

    Is there a solution to this? Experiencing the same problem.

Viewing 5 posts - 1 through 5 (of 5 total)

You must be logged in to reply to this topic.