FLIR One Developer / Blog / Topics / cat s60 / CAT S60, IOException at Camera.connect( … )

CAT S60, IOException at Camera.connect( … )

Home Forums FLIR Mobile SDK Development Android Development CAT S60, IOException at Camera.connect( … )

Tagged: 

This topic contains 2 replies, has 2 voices, and was last updated by Profile photo of Mario Mario 2 months, 3 weeks ago.

Viewing 3 posts - 1 through 3 (of 3 total)

  • Author

    Posts

  • #12044

    Profile photo of Mario
    Mario

    Participant

    Dear Support,

    I’m working with a CAT S60 and want to connect to the integrated Flir camera. Therefore, I slightly changed the example from Flir to also discover the integrated S60_CAMERA identity. This works well so far, the integrated cam is discovered with deviceId=”S60_CAMERA”.

    If then in the next step I try to connect to the camera with Camera.connect( … ) I get an exception

    “Could not connect: java.io.IOException: Unsupported camera type”

    I did research quite a while for examples to work with the CAT S60 but I did not find anything valuable.

    Is there maybe an example someone can provide for starting to work with the CAT S60?

    Thank you in advance,
    mario

    #12048

    Profile photo of Gavin
    Gavin

    Keymaster

    Hi Mario,

    Are you using the Mobile SDK?

    Gavin

    #12050

    Profile photo of Mario
    Mario

    Participant

    Hi Gavin,
    I use the newest downloadable SDK with the two files
    androidsdk-release.aar, and
    thermalsdk-release.aar.
    in the example project
    FlirOneCamera
    As I read in the page “Android Platform Guide – FLIR One/Cat S60” this SDK should also work for the Cat S60.
    Is there any hint you could provide for getting it work?
    Thank you in advance for your help!
    mario

Viewing 3 posts - 1 through 3 (of 3 total)

You must be logged in to reply to this topic.