FLIR One Developer / Blog / Topics / temperature android range max / Changing temperature range the camera can detect

Changing temperature range the camera can detect

Home Forums FLIR ONE SDK Development Android development Installation and getting started Changing temperature range the camera can detect

This topic contains 2 replies, has 3 voices, and was last updated by Profile photo of maya maya 6 months, 3 weeks ago.

Viewing 3 posts - 1 through 3 (of 3 total)

  • Author

    Posts

  • #9518

    Profile photo of Enrique
    Enrique

    Participant

    Hello, how can one change the temperature range the FLIR one camera can detect? It seems to have a set upper range it can detect, but I’d like to deal with higher temperatures. I know this can be done on the main FLIR one app.

    #9521

    Profile photo of Ava
    Ava

    Participant

    A camera’s temperature range and sensitivity are important considerations, too. The range tells you what the minimum and maximum temperatures are that the camera can measure Popeyes Survey

    #11689

    Profile photo of maya
    maya

    Participant

    FLIR One Tech Specs states the camera can detect temperature differences down to 0.1°C. However, detecting temperature differences and measuring temperatures are two very different things TellPopeyes

Viewing 3 posts - 1 through 3 (of 3 total)

You must be logged in to reply to this topic.