FLIR One Developer / Blog / Topics / android, flir gen 2, synchronization issues / Concurrency issues with RenderedImage and android threadpool

Concurrency issues with RenderedImage and android threadpool

Home Forums FLIR developer community General discussion Concurrency issues with RenderedImage and android threadpool

This topic contains 0 replies, has 1 voice, and was last updated by Profile photo of Amit Amit 2 years ago.

Viewing 1 post (of 1 total)

  • Author

    Posts

  • #7675

    Profile photo of Amit
    Amit

    Participant

    I am using android’s thread pool executor framework (initialized as below).

    
    BlockingQueue<Runnable> taskQueue = new LinkedBlockingQueue<>();
    ExecutorService executorService = new ThreadPoolExecutor(totalCores, totalCores * 3, 10, TimeUnit.SECONDS, taskQueue);
    

    Now, consider the following function onFrameProcessed –

    
    public void onFrameProcessed(RenderedImage renderedImage) {
    String timeNow = new SimpleDateFormat("d-M-Y_HH_mm_ss_SSS").format(new Date()).toString();
    CustomRunnable3 customRunnable3 = new CustomRunnable3(renderedImage, timeNow);
    executorService.execute(customRunnable3);
    }
    

    Definition of CustomRunnable3 is as follows:

    
    class CustomRunnable3 implements Runnable {
        RenderedImage renderedImageLocal;
        String basePath, timeNowCopy;
        int hashCode;
    
        CustomRunnable3(RenderedImage renderedImage, String timeNow) {
            renderedImageLocal = renderedImage;
            this.basePath = Environment.getExternalStoragePublicDirectory(Environment.DIRECTORY_PICTURES).toString();
            this.timeNowCopy = timeNow;
            hashCode = renderedImageLocal.hashCode();
        }
    
        @Override
        public void run() {
            if (renderedImageLocal.imageType() == RenderedImage.ImageType.ThermalRadiometricKelvinImage) {
                int[] thermalData = renderedImageLocal.thermalPixelValues();
                String dataPath = basePath + "/" + this.timeNowCopy + ".csv";
                try {
                    PrintWriter printWriter = new PrintWriter(dataPath);
                    int dataLen = thermalData.length;
                    for (int i = 0; i < dataLen; i++) {
                        printWriter.println(thermalData[i]);
                    }
                    printWriter.close();
                } catch (IOException e) {
                    e.printStackTrace();
                }
                String imgPath = basePath + "/" + this.timeNowCopy + ".jpg";
                try {
                    if (hashCode != renderedImageLocal.hashCode()) {
                        Log.e("Checking", "Hash code changed..");
                    }
                    renderedImageLocal.getFrame().save(new File(imgPath), frameProcessor);
                    if (hashCode != renderedImageLocal.hashCode()) {
                        Log.e("Checking", "Hash code changed after writing..");
                    }
                } catch (IOException e) {
                    e.printStackTrace();
                }
    
            }
        }
    }
    

    Usage Scenario : onFrameReceived is being called multiple times per second(like 4-5 times). In each call to onFrameReceived, I am saving two files from renderedImage object (1 csv file, 1 jpg file). Both of these files must be related to each other because both are created from one parent and have same name(except the extension).

    Problem : But that is not happening and somehow I am ending up with jpg file content from 1 renderedImage and csv content from another renderedImage object. What are the possible reasons for this problem, please share your opinion.

Viewing 1 post (of 1 total)

You must be logged in to reply to this topic.