FLIR One Developer / Blog / Topics / xamarin / couldn't find libsystemimage.so

couldn't find libsystemimage.so

Home Forums FLIR ONE SDK Development Android development Installation and getting started couldn't find libsystemimage.so

Tagged: 

This topic contains 8 replies, has 6 voices, and was last updated by Profile photo of James James 2 months ago.

Viewing 9 posts - 1 through 9 (of 9 total)

  • Author

    Posts

  • #5233

    Profile photo of philippe
    philippe

    Participant

    Hi,

    I use the FLIR SDK on a S60 using Xamarin (C#).
    The lib import work great, I could see the reference, but when I create a FrameProcessor, the compilation work but throw an error when running : couldn’t find libsystemimage.so

    Do you have any idea to solve this problem?

    Regards,
    Philippe

    #5263

    Profile photo of Ian Butler
    Ian Butler

    Participant

    Can you check if libsystemimage.so is being put in your apk file? You can unzip the apk and search for the file. There might be a Xamarin-specific issue for making sure native libraries make it from an aar to the apk. I would recommend posting in a Xamarin forum or Stack Overflow about the issue as well.

    #5288

    Profile photo of philippe
    philippe

    Participant

    Hi Ian,

    when I look inside the APK, i could find libsystemimage.so in the folder \lib\armeabi-v7a\.
    It seems that is not a link problem.

    When I compile, I have the error :

    dalvik.system.PathClassLoader[DexPathList[[zip file "/data/app/EZPlan.Droid.EZPlan.Droid-1/base.apk"],nativeLibraryDirectories=[/data/app/EZPlan.Droid.EZPlan.Droid-1/lib/arm64, /data/app/EZPlan.Droid.EZPlan.Droid-1/base.apk!/lib/arm64-v8a, /vendor/lib64, /system/lib64]]] couldn't find "libsystemimage.so"

    If I rename the folder JNI\armeabi-v7a in JNI\arm64-v8a in the AAR, I got this error :

    dlopen failed: "/data/app/EZPlan.Droid.EZPlan.Droid-1/lib/arm64/libsystemimage.so" is 32-bit instead of 64-bit

    So I think the AAR is not complete.
    What do you think ?

    Best regards,
    Philippe

    #6305

    Profile photo of John
    John

    Participant

    Is there a resolution to this problem? I am having this same problem building a Java app with Android Studio 3.1.1. If it matters I am on a mac, though I am seeing the issue as Phillipe is. There is a libSystemImage.so and libmbwrapper.so in armeabi-v7a, but not in the arm64-v8a folder.

    I don’t think this has anything to do with C# or Xamarin.

    • This reply was modified 2 years, 5 months ago by Profile photo of John John. Reason: Pointing out this happens in Android Studio too

    #6307

    Profile photo of John
    John

    Participant

    So I built the sample app and it ran on my dev phone which led me to more investigation. After unzipping it I found the same libraries as my app has but no folders for other architectures. My app uses a few other libraries, the main one being OpenCV, and they all provide 64 bit versions. As an experiment I removed the 64 bit libraries, rebuilt, and the app runs. Or it runs at least as far as the Flir camera initialization. Now I’ll have to test OpenCV and see if it will work.

    Even if this workaround keeps me going for a while I’d still much rather have a 64 bit version of the Flir library. Working with images it makes sense to take advantage of everything the new processors can do. Is this in the works?

    #6308

    Profile photo of philippe
    philippe

    Participant

    Hi John,

    I stop investigating in flir and android, so I couldn’t help you, sorry.
    Good luck.

    Regards,
    Philippe

    #7815

    Profile photo of Charles
    Charles

    Participant

    I have the same problem. After I imported the latest version of OpenCV (following the instruction at ), I got this error couldn’t find “libsystemimage.so” every time when I tried to run the app. This is because the so file wasn’t copied to the APK after the so files from OpenCV were copied to the /app/src/main/jniLibs folder as instructed. I have spent almost a day on troubleshooting this issue with no luck.

    Has anyone run into this issue? It seems OpenCV is very relevant to thermal image analysis. I would appreciate if someone can enlighten me.

    #12222

    Profile photo of Marek
    Marek

    Participant

    Same problem, but honestly I have no idea where to find libsystemimage.so, it is not being added to apk. Any advice?

    • This reply was modified 3 months ago by Profile photo of Marek Marek.

    #12738

    Profile photo of James
    James

    Participant

    I have run the same issue. That instruction is OK. You just need some extra information. First, please read here about spying apps and you’ll be able to solve this issue with non-copying files

Viewing 9 posts - 1 through 9 (of 9 total)

You must be logged in to reply to this topic.