FLIR One Developer / Blog / Topics / EGL_BAD_SURFACE libEGL / EGL_BAD_SURFACE errors Android

EGL_BAD_SURFACE errors Android

Home Forums FLIR developer community General discussion EGL_BAD_SURFACE errors Android

This topic contains 16 replies, has 8 voices, and was last updated by Profile photo of Larinni Larinni 8 months, 3 weeks ago.

Viewing 17 posts - 1 through 17 (of 17 total)

  • Author

    Posts

  • #6243

    Profile photo of Devrim
    Devrim

    Participant

    Hello
    Is there any idea about the reasons of these EGL_BAD_SURFACE errors and possible solutions ? The errors are randomly observed. I can observe them in the reference Android app too.
    Thanks

    1- flironeexampleapplication E/libEGL: eglQuerySurface:714 error 300d (EGL_BAD_SURFACE)

    2- flironeexampleapplication E/libEGL: eglMakeCurrent:945 error 300d (EGL_BAD_SURFACE)

    #6244

    Profile photo of Dominique
    Dominique

    Moderator

    Hello Infrared Developer,

    Would you please tell us what phone and FLIR One you are using?

    Thank you,
    Dominique Strauss

    #6256

    Profile photo of Devrim
    Devrim

    Participant

    I observe the problem with Samsung SM-T810 Tablet PC, Android 5.0.2, API 21 device. Error rate is high with FLIR ONE GEN2 and relatively lower with FLIR ONE GEN3. (I read about similar problems in big screen resolution but I am not sure)

    • This reply was modified 2 years, 1 month ago by Profile photo of Devrim Devrim.

    #6258

    Profile photo of Dominique
    Dominique

    Moderator

    Hi Infrared Developer,

    Thank you for providing that information. that particular device isn’t currently on the list of Android devices we’ve tested and confirmed to be compatible with the FLIR ONE. We are in the process of testing additional devices, and in the meantime we recommend that you use one of those currently on the compatibility list:

    http://flir.eu/flirone/android/?bvstate=pg:10/ct:q

    http://www.flir.tw/flirone/support/compatibility/

    It is very likely that there is a tablet GPU incompatibility with the FLIR One.

    Do you have any of the devices listed above?

    Please let us know if you have any other questions.

    Thank you,
    Dominique Strauss

    #6259

    Profile photo of Devrim
    Devrim

    Participant

    Thank you Dominique. I can especially go on development with Samsung Galaxy S6 edge+ SM-G928I specs – SamMobile. The rate is very low with Gen 3.

    Anyway, could you tell me the reasoning of the EGL_BAD_SURFACE type errors ? Could it be a workaround ?

    #6274

    Profile photo of Dominique
    Dominique

    Moderator

    Hi Devrim,

    Unfortunately we do not currently have a workaround.

    We are continuing to work on adding to our compatibility list

    Thank you,
    Dominique Strauss

    #6290

    Profile photo of Devrim
    Devrim

    Participant

    Dominique, thank you for your comments.
    Anohter point is that the official FLIR ONE application is running very robust on Samsung SM-T810 Tablet PC device. I think, the official app already has a workaround in it. Could you comment on this ?

    #6294

    Profile photo of Peter
    Peter

    Participant

    Hi!

    I’ve got the same problem on CATS60. The same problem is FlirOne example application. GLSurfaceView instance lost EGL context. There is interesting if GLSurfaceView OnPause is not used in app. lifcycle, GLSurfaceView works correctly after re-enter screen off via power button.

    #6296

    Profile photo of Dominique
    Dominique

    Moderator

    Hi Peter and Devrim,

    We are continuing to look into this. We will keep you posted on the progress.

    Thank you,
    Dominique Strauss

    #7131

    Profile photo of
    Anonymous

    Could be that the EGL context isn’t set up right. Are you missing a makeCurrent() somewhere? If you’re running this in the UI thread you may need to make the EGL context current more often, as the UI thread may be using GLES for its own rendering.

    • This reply was modified 1 year, 11 months ago by Profile photo of Allison Allison.

    #7150

    Profile photo of Devrim
    Devrim

    Participant

    Hi Anonymous,
    Could you make your comment more clear please ?

    #7987

    Profile photo of Carlos Manuel
    Carlos Manuel

    Participant

    I have the same problem when my app goes to background and then resumed. Dominique you speak about compatibilily but the official Flir ONE app, from the playstore, works perfectly in the two devices that i tested, that these devices are not in the compatibilty list that you share, and the sample application that comes with the SDK fails too when apply the previous process. I you are able to share the source code of that app i think that will be better.

    Devices:
    Samsung Galaxy S6: SM-G920P OS: Android 7.0
    KYOCERA: E6820TM OS: 6.0.1

    Flir:
    Flir One Gen 3 for android devices.

    #8028

    Profile photo of Allison
    Allison

    Moderator

    Hi Carlos

    Unfortunately, we cannot share the source code for the app. Additionally, we generally see GLSurface issues like EGL_BAD_SRFACE because of how some phone’s GPU’s handle the GLSurface. I can suggest looking into these solutions https://developer.flir.com/forums/topic/recover-the-device-connection/
    If the issue persist past those solutions, I can escalate the issue and see if we can find a different solution for you.

    Thank you,
    Allison Torchia

    #8038

    Profile photo of Carlos Manuel
    Carlos Manuel

    Participant

    I understand the thing with the source code, the thing that i dont understand is why the app that comes with the SDK didn’t work and the one in the play store works fine, i think that the sample app sould be fixed. Don’t you think so?

    #8053

    Profile photo of Vlad
    Vlad

    Participant

    What are the solutions for this issue?

    #8164

    Profile photo of Vlad
    Vlad

    Participant

    Have there been any improvements in this issue?

    #9957

    Profile photo of Larinni
    Larinni

    Participant

    The problem persists. Any solution for that?

Viewing 17 posts - 1 through 17 (of 17 total)

You must be logged in to reply to this topic.