Home › Forums › FLIR Mobile SDK Development › Android Development › images is to slow
Tagged: thermal-sdk-android performance
This topic contains 8 replies, has 5 voices, and was last updated by Lynne 3 months, 3 weeks ago.
Viewing 9 posts - 1 through 9 (of 9 total)
-
Author
Posts
-
Participant
I use sample program from thermal-sdk-android-java-1.0.5 to connect FLIRONE pro and I got the picture.But the image has a delay of about 2 seconds and 4 frames per second.How do I reduce the delay and increase the frame rate.The Compile Sdk version in the Project Structure is API 28: Android 9.0 (Pie).
KeymasterHi Sun,
I’ve escalated this issue internally to our technical support staff. Hopefully I can get back to you in 2-3 days.
Thanks for your patience,
Gavin
FLIR Community SupportParticipantHi Gavin:
Is there any new progress on this issue?Thanks
ParticipantHi Gavin:
I have upgraded my project from the legacy SDK to the latest one (1.1.1).
We used a thread pool to get ThermalImage and optimize the frame rate, but the program often crashed.
Must “ThermalImage” be obtained in a single thread?
Thanks!ParticipantHi sun,
May I see how you managed to optimize the frame rate using the thread pool?
Thanks!ParticipantUnfortunately there are several performance issues with FLIR’s Android SDK.
We have tested on a variety of hardware and frame rates fall below 2 FPS on even quite powerful Android devices.
Modern phones and tablets can maintain 8+ FPS, but Android TV boxes struggle to manage over 2 FPS. Even the Nvidia Shield can only achieve 4 FPS!
On poorly performing devices, there is nothing you can do to improve the frame rate. Before performing any processing, the frame rate is already under 2 FPS.
Doing nothing in onImageReceived() – 6 FPS
camera.withImage() … then image.getImage() – 1.9 FPSAfter spending several days on this I have come to the conclusion that there is either a strange USB connection performance issue with some devices or a bug in the SDK.
If anyone can shed any light on this issue, it would be much appreciated.
KeymasterHey Michael,
What camera are you testing on?
Thank you,
Gavin
FLIR Community SupportParticipantThis question is about the SDK and applies to all FLIR hardware. (Tested with FLIR ONE PRO and FLIR ONE PRO LT on many Android devices)
Most Android devices can not achieve anywhere near 9fps.
There is a bug in the SDK that results in frames being dropped because the SDK developer (falsely) assumed buffers would align with frames. In reality there may be more or less than 1 frame in a buffer – so this bug is dependent on how Android and USB comms fills the buffers.
Easy to fix, but from what I can see, this has been a problem since day one.
If anyone from FLIR wants help to fix this, please get in touch.
The only other alternative is to avoid FLIRs SDK and write your own implementation based on the hardware information found on eevblog.
Participantwow. That is terrible
-
Author
Posts
Viewing 9 posts - 1 through 9 (of 9 total)
You must be logged in to reply to this topic.