FLIR One Developer / Blog / Topics / FLIR One, FLIR One GEN 3, frame, general, pixels, renderimage, thermal pixels, thermal value / Measurement Range and Distance of flir one for andorid gen3 camera

Measurement Range and Distance of flir one for andorid gen3 camera

Home Forums FLIR developer community General discussion Measurement Range and Distance of flir one for andorid gen3 camera

This topic contains 3 replies, has 4 voices, and was last updated by Profile photo of Foster Foster 1 year, 1 month ago.

Viewing 4 posts - 1 through 4 (of 4 total)

  • Author

    Posts

  • #7386

    Profile photo of surendra
    surendra

    Participant

    hi can any one tried measuring negative temperatures with FLIR One and a distance up to which can it measure accurately?

    #7396

    Profile photo of Allison
    Allison

    Moderator

    Hi Surendra,

    The FLIR One can measure temperatures from -20 °C to 120 °C (-4 °F to 248 °F) so it should be able to measure negative temperatures up to -20 °C. For accurate temperature readings, the maximum distance is about 50 yards in perfect atmospheric conditions (no rain, clouds or humidity). The detection passed 50 yards may not be accurate, however, you may still manage to detect some heat signatures which would tell you if the object is warmer or colder relative to its surroundings.

    Please keep in mind emissivity of the objects will affect temperature readings as well as gain mode if you have a Pro model.

    Thank you,
    Allison Torchia

    • This reply was modified 1 year, 11 months ago by Profile photo of Allison Allison.

    #8496

    Profile photo of Paige
    Paige

    Participant

    Thermal cameras, like visible cameras can see as far as your eye can see in most cases. Whether you will “see something” at a given distance depends on the size of the size of the object and the contrast walgreenslistens.

    #8791

    Profile photo of Foster
    Foster

    Participant

    FLIR ONE offers non-contact spot temperature measurement, patented MSX Technology and the house, FLIR ONE’s thermal camera gives you a new view of your everyday world bluestacks.

Viewing 4 posts - 1 through 4 (of 4 total)

You must be logged in to reply to this topic.