FLIR One Developer / Blog / Topics / Measuring +200C temp with Flir camera in S60?

Measuring +200C temp with Flir camera in S60?

Home Forums FLIR ONE SDK Development Device specific CAT S60/S61 smartphones Measuring +200C temp with Flir camera in S60?

This topic contains 0 replies, has 1 voice, and was last updated by Profile photo of Jaan Jaan 2 years, 8 months ago.

Viewing 1 post (of 1 total)

  • Author

    Posts

  • #6005

    Profile photo of Jaan
    Jaan

    Participant

    Hi,

    I’m using the S60 to record asphalt temperatures before pavement. The maximum temperature I can measure/record with the S60 Flir application is about +145 C but I need to record up to and over +200 C. Is the Flir camera in S60 able to measure and record surface temperature of +200 C? If yes, then how can I take photos showing with temperature measurement of up to +200 C?

    Best Regards,
    Jaan Saar

Viewing 1 post (of 1 total)

You must be logged in to reply to this topic.