FLIR Mobile Developer / Blog / Topics / legacy sdk / Migrating from legacy SDK

Migrating from legacy SDK

Home Forums FLIR Mobile SDK Development Android Development Migrating from legacy SDK

Tagged: 

This topic contains 6 replies, has 5 voices, and was last updated by Profile photo of Yurii Yurii 7 months, 2 weeks ago.

Viewing 7 posts - 1 through 7 (of 7 total)

  • Author

    Posts

  • #12270

    Profile photo of Rafał
    Rafał

    Participant

    How long did it take you to migrate from the legacy Flir Android SDK to the newest?

    #14688

    Profile photo of Dani
    Dani

    Participant

    It depends on the amount of functionalities you use. The implementations are very different

    Dani

    #16556

    Profile photo of erick
    erick

    Participant

    Can you send me the legacy sdk? Im having a problem with the new one and I can’t find the legacy to download geral@erick.pt thank you!

    #16574

    Profile photo of Gavin
    Gavin

    Keymaster

    Hello Erick,

    Could you please submit a request for the Legacy SDK to .

    In this request please include your name, email, and a description of your app that you intend to create.

    Best,
    Gavin
    FLIR Community Support

    #16767

    Profile photo of erick
    erick

    Participant

    I have now the Legacy SDK (3.1.5), but I’m having a problem. the app crash in the second time I open the camera. That problem keeps occurring even in the example inside the SDK you send. It’s an SDK problem or implementation? Can you help me?

    #16813

    Profile photo of Gavin
    Gavin

    Keymaster

    Hi Erick,

    Which camera are you using?

    Gavin
    FLIR Community Support

    #17991

    Profile photo of Yurii
    Yurii

    Participant

    Hi, Gavin.
    I am experiencing same problem as erick.
    Both the sample project and my app are crashing right after thermal camera is connected. Xcode 12, Flir One Pro. Could you please advice on what the possible solution might be?. The stacktrace is the following:

    #0 0x0000000104ce42ac in cv::UMatData::~UMatData() ()
    #1 0x0000000104a78398 in cv::StdMatAllocator::deallocate(cv::UMatData*) const ()
    #2 0x000000010452b6f4 in atlas::filterChain::CPUVBM4DDenoiseFilter::bufferNoiseEstCoeffs(float*, float const*, int, int, int) ()
    #3 0x000000010452ab9c in atlas::filterChain::CPUVBM4DDenoiseFilter::noiseEstimationModule(float const*, int, float const*, float const*, float*, float*, int, int, float, bool) ()
    #4 0x0000000104529ac4 in atlas::filterChain::CPUVBM4DDenoiseFilter::denoiseVBM4D(float*, int, float, float&, float&, float const*, float const*, bool, bool, float*, int, float*, int, int, int) ()
    #5 0x0000000104529364 in atlas::filterChain::CPUVBM4DDenoiseFilter::update(void*, unsigned long, char const*) ()
    #6 0x000000010457d2fc in atlas::filterChain::OutputPin::deliver(void*, unsigned long) ()
    #7 0x000000010451fe70 in atlas::filterChain::CPUTemporalRowColumnNoiseSuppressionFilter::update(void*, unsigned long, char const*) ()
    #8 0x000000010457d2fc in atlas::filterChain::OutputPin::deliver(void*, unsigned long) ()
    #9 0x0000000104519c5c in atlas::filterChain::CPUReplaceDeadPixelsFilter::update(atlas::filterChain::CPUBuffer*, atlas::filterChain::CPUBuffer const*) ()
    #10 0x0000000104519a44 in atlas::filterChain::CPUReplaceDeadPixelsFilter::update(void*, unsigned long, char const*) ()
    #11 0x000000010457d2fc in atlas::filterChain::OutputPin::deliver(void*, unsigned long) ()
    #12 0x000000010457cbd8 in atlas::filterChain::SplitFilter::update(void*, unsigned long, char const*) ()
    #13 0x000000010457f160 in atlas::filterChain::Pipeline::update(void*, unsigned long, char const*) ()
    #14 0x000000010457dfe8 in atlas::filterChain::GLPipeline::update(void*, unsigned long, char const*) ()
    #15 0x000000010457f160 in atlas::filterChain::Pipeline::update(void*, unsigned long, char const*) ()
    #16 0x000000010457dfe8 in atlas::filterChain::GLPipeline::update(void*, unsigned long, char const*) ()
    #17 0x00000001044da30c in -[FLIROneSDKStreamManager drawInRect:] at /Users/ibutler/Documents/Code/FLIR/flirone-ios-sdk/FLIROneSDK/FLIROneSDK/FLIROneSDKStreamManager.mm:2760
    #18 0x00000001044d8058 in -[FLIROneSDKStreamManager FLIRRosebudDidReceiveFrame:] at /Users/ibutler/Documents/Code/FLIR/flirone-ios-sdk/FLIROneSDK/FLIROneSDK/FLIROneSDKStreamManager.mm:2481

    #19 0x000000018840c0f0 in __NSThread__start__ ()
    #20 0x00000001cef99ca8 in _pthread_start ()

Viewing 7 posts - 1 through 7 (of 7 total)

You must be logged in to reply to this topic.