FLIR One Developer / Blog / Topics / temperature / Saving Temperature Matrix

Saving Temperature Matrix

Tagged: 

This topic contains 11 replies, has 5 voices, and was last updated by Profile photo of 志成 志成 1 year, 6 months ago.

Viewing 12 posts - 1 through 12 (of 12 total)

  • Author

    Posts

  • #5197

    Profile photo of Natan
    Natan

    Participant

    Hello,
    I’m looking into saving the temperature matrix (kelvin) to a file. i was expecting to have an array of 60X80 but i get 320X240 . I there a way to downsample it to the original sensor values ?

    if somebody have done the downsample or have saved the temperature matrix i would like to learn how to do it.

    regards,
    Nati

    #5198

    Profile photo of Natan
    Natan

    Participant

    In addition , why output of the thermalpixels looks like the one of my profile picture?

    #5199

    Profile photo of Tim Liew
    Tim Liew

    Moderator

    Hi Natan,

    The radiometric image should be 320*240, while the visual image is scaled up by a factor of two. As for the thermal image you are getting, is that the thermal image you get from the FLIR One app?

    Best,
    Tim

    #5220

    Profile photo of Natan
    Natan

    Participant

    Hi Tim,
    Thanks for the replay.
    I have saved the Temperature matrix using BufferedOutputStream into a txt file . I get a 320X240 temperature data but it’s saving it very slow 2 second per frame (each file gets the date and time name)..

    in general my aim is to save temperature data continually with the least leg possible.

    Is there a better way to record temperature matrix data into my sd card ?

    Will it be faster to upload the matrix to a server ?

    #5226

    Profile photo of Tim Liew
    Tim Liew

    Moderator

    You could try threading to handle the saving, or I would suggest saving it differently instead of each frame creating and writing a new file which may be producing some lag.

    #5290

    Profile photo of Natan
    Natan

    Participant

    thanks for the reply ,
    i have used threading and it’s working well.

    #5295

    Profile photo of Tim Liew
    Tim Liew

    Moderator

    No problem, glad you got it worked out.

    #6331

    Profile photo of ARKA
    ARKA

    Participant

    Hello Natan,

    Could you able to save temperature matrix corresponding to radiometric jpeg/data at actual streaming rate? Can you share the portion of the code that does the trick? It will be of great help.

    Thank you

    #6332

    Profile photo of Natan
    Natan

    Participant

    Contact me in privet i would send you a java file (i havent working on this project for a long time) . so you could read and grab what ever you need

    #6334

    Profile photo of ARKA
    ARKA

    Participant

    Thank you very much for your help. My email id is arkabhowmik(at)yahoo(dot)co(dot)uk.

    #7687

    Profile photo of Amit
    Amit

    Participant

    Hey guys,
    could you please share that multi threaded code to save thermal data matrix in files. I am having an issue with saving jpg and thermal data from each frame. My email id is amit.sharma1262@gmail.com

    #8440

    Profile photo of 志成
    志成

    Participant

    Hello Natan,
    I have the same problem.Could you share the portion of the code that does the trick? It will be of great help. My email id is 1085437068@qq.com

    Thank you

Viewing 12 posts - 1 through 12 (of 12 total)

You must be logged in to reply to this topic.